AXIS#.MT.CLEAR

Description

AXIS#.MT.CLEAR clears a motion task from the drive. This command needs one argument in order to clear a motion task. A motion task consists of the following parameters:AXIS#.MT.P, AXIS#.MT.V, AXIS#.MT.CNTL, AXIS#.MT.ACC, AXIS#.MT.DEC, AXIS#.MT.MTNEXT, AXIS#.MT.TNEXT

Example

Clears motion task number 5:

-->AXIS1.MT.CLEAR 5

After performing this command the drive displays the following:

5   0.000 Counts   0.000 rpm   0   0.000 rpm/s   0.000 rpm/s   0   0   0 ms

A value of 0 for velocity, acceleration, or deceleration displays motion task as uninitialized.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Command Array

Units

N/A

Range

0 to 31
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
AXIS1.MT.CLEAR

6301

189D

Unsigned8[32]

Read/Write

-

AXIS2.MT.CLEAR

71837

1189

Unsigned8[32]

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MT.CLEAR

6301

Unsigned8[32]

Read/Write

-

Related Topics

Motion Tasks